Investor Relations

Email Alerts

Email Address *
Mailing Lists *



Contact IR

Institutional Investors:
Direct Line: 610-893-9435
Click Here to Email

Address:
TE Connectivity
1050 Westlakes Drive
Berwyn, PA 19312

TE Connectivity Main Switchboard:
US 610-893-9800

Connect With Us

TE Connectivity's PolyZen YC Series Wins EDN China's 2015 Innovation Award for Best Passive Component

July 22, 2015

MENLO PARK, Calif., July 22, 2015 /PRNewswire/ -- TE Connectivity's (TE) business unit, TE Circuit Protection, has been named a winner of EDN China's 2015 Innovation Awards for its PolyZen YC device series. Winning in the "Passive Component" category, TE's hybrid PolyZen YC devices offer a highly integrated approach to helping protect consumer electronics from damage caused by electrostatic discharge and other electrical over-stress events.

TE Connectivity logo.

The PolyZen ZEN056V230A16YC and ZEN056V260A16YC devices combine a precision Zener diode and a resettable PolySwitch PPTC (polymer positive temperature coefficient) device in a compact (4.0mm x 5.0mm x 1.3mm) package. A PolyZen device's Zener diode is thermally connected to the PPTC device to enable rapid heat transfer, which in turn allows the PPTC device to react faster, thus enhancing protection. A single hybrid PolyZen YC device can help protect products against damage caused by overvoltage, overcurrent, reverse-bias, ESD and overtemperature events more effectively than solutions that use multiple discrete devices. Typical applications include tablets, set-top boxes, hard disk drives and DC power ports.

"We are delighted that EDN China has recognized our PolyZen YC series as the best passive component of 2015," said Jin Xu, Product Manager, TE Circuit Protection. "These hybrid devices enable a single-component implementation for efficient SMT-line production and offer all the advantages of helping to reduce board space, lower bill-of-materials costs and speed time to market. It is an honor to have our product win this prestigious industry award."

ABOUT TE CONNECTIVITY

TE Connectivity (NYSE: TEL) is a $13 billion world leader in connectivity. The company designs and manufactures products at the heart of electronic connections for the world's leading industries including automotive, energy and industrial, broadband communications, consumer devices, healthcare, and aerospace and defense. TE Connectivity's long-standing commitment to innovation and engineering excellence helps its customers solve the need for more energy efficiency, always-on communications and ever-increasing productivity. With nearly 90,000 employees in over 50 countries, TE Connectivity makes connections the world relies on to work flawlessly every day. To connect with the company, visit: www.te.com.

Contacts:   

Media Relations:      

Media Relations:


Matthew Bucklin

Jin Xu


TE Connectivity

TE Connectivity


(650) 361-2089

(+86) 21 61067308


matthew.bucklin@te.com

jin_xu@te.com

 

Logo - http://photos.prnewswire.com/prnh/20110505/LA96464LOGO

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/te-connectivitys-polyzen-yc-series-wins-edn-chinas-2015-innovation-award-for-best-passive-component-300116458.html

SOURCE TE Connectivity