Investor Relations

Email Alerts

Email Address *
Mailing Lists *



Contact IR

Institutional Investors:
Direct Line: 610-893-9435
Click Here to Email

Address:
TE Connectivity
1050 Westlakes Drive
Berwyn, PA 19312

TE Connectivity Main Switchboard:
US 610-893-9800

Connect With Us

Jade Communications Selects TE Connectivity Powered Fiber Cable System For Large HD Camera Deployment

June 02, 2015

PoE Extender and Powered Fiber Cable Connect HD Cameras at Golf Course

MINNEAPOLIS, June 2, 2015 /PRNewswire/ -- TE Connectivity (TE), a world leader in connectivity, today announced that Jade Communications of Boca Raton, Fla. has designed in TE's powered fiber cable system and PoE extender to slash deployment costs at a golf course. The 36-camera system at a south Florida golf course, with cameras located up to 10,700 feet from the power source, was initially designed with dedicated fiber and power runs to each camera. By designing the system with TE's powered fiber cable system and PoE extender, however, Jade Communications was able to save $142,000 (14.5 percent) in network build-out costs.

TE Connectivity's powered fiber cable system PoE extender

TE's powered fiber cable system provides a complete rack-to-device vision for both powering and communicating with network access devices such as small cells, HD cameras and Wi-Fi access points. The powered fiber cable system eliminates the complexity of device installation and allows devices like Wi-Fi access points or HD cameras to be placed exactly where they are needed for maximum effectiveness by combining power and optical fiber communications into one system. The powered fiber cable system is powered by a centrally located, 48V DC, NEC Class II and SELV compliant power supply.

The PoE extender is a small device that incorporates electrical power management, circuit protection electronics, and an optical-to-electrical media converter in an environmentally sealed enclosure. The PoE extender device terminates the powered fiber cable in a weatherproof housing, and provides a single RJ45 jack output for PoE/PoE+ output. Featuring plug-and-play installation, the PoE extender is a simple, unobtrusive way to deploy PoE devices in large buildings or urban or suburban areas.

"Our powered fiber cable system and PoE extender were designed to reduce deployment costs and bring power and connectivity to devices up to two miles away from the power source," said Mark Hesling, global vice president of Product Management at TE Connectivity. "It is an ideal solution for this golf course application, and well-suited for deployments in urban centers and campuses where installers want to save money and time by delivering PoE power and Gigabit speed connectivity in the same cable."

ABOUT TE CONNECTIVITY

TE Connectivity (NYSE: TEL) is a $14 billion global technology leader. Our connectivity and sensor solutions are essential in today's increasingly connected world. We collaborate with engineers to transform their concepts into creations – redefining what's possible using intelligent, efficient and high-performing TE products and solutions proven in harsh environments. Our 80,000 people, including 7,500 design engineers, partner with customers in over 150 countries across a wide range of industries. We believe EVERY CONNECTION COUNTS – www.TE.com.   

TE Connectivity, TE connectivity (logo), TE (logo) and EVERY CONNECTION COUNTS are trademarks.
All other logos, products and/ or company names referred to herein might be trademarks of their respective owners.
© 2015 TE Connectivity Ltd. family of companies. All Rights Reserved.

Contacts:

Media Relations:


Colleen Murphy-Gomez


TE Connectivity


952-917-0279


colleen.murphygomez@te.com



TE Connectivity

Photo - http://photos.prnewswire.com/prnh/20150518/217284 

Logo - http://photos.prnewswire.com/prnh/20150122/170890LOGO

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/jade-communications-selects-te-connectivity-powered-fiber-cable-system-for-large-hd-camera-deployment-300086392.html

SOURCE TE Connectivity