Investor Relations

Email Alerts

Email Address *
Mailing Lists *



Contact IR

Institutional Investors:
Direct Line: 610-893-9435
Click Here to Email

Address:
TE Connectivity
1050 Westlakes Drive
Berwyn, PA 19312

TE Connectivity Main Switchboard:
US 610-893-9800

Connect With Us

TE Connectivity Launches MRJ21 XG 10 GbE Copper Cabling System for Superior Data Center Agility

September 17, 2012

Pre-Terminated Cabling Solution Delivers Unparalleled 10 GbE Throughput While Consuming up to 37% Less Space Than Traditional Twisted Pair Systems

GREENSBORO, N.C.--(BUSINESS WIRE)--Sep. 17, 2012-- TE Connectivity Ltd. today announced its new MRJ21 XG pre-terminatedcopper cabling system designed to deliver 10 GbE (10-Gigabit Ethernet) throughput in all architectures where copper cabling is required. Based on the foundation of TE’s industry-leading MRJ21 high-density interface, the MRJ21 XG cabling solution helps facilitate management of data center rack and floor space, density and throughput while also capitalizing on its ease of deployment and fast installation rates.

“Due to the increasing penetration of 10GBASE-T switches and blades in the data center, the need to quickly deploy a 10 GbE copper system with minimal white space consumption has become critical,” said  Kam Patel , business line manager of data center solutions atTE Enterprise Networks. The MRJ21 XG cabling system, comprised of cable assemblies, cassettes and Cat 6A shielded patch cords, answers this challenge in three ways:

  • Space savings – the unique MRJ21 XG trunk cable typically consumes 5% less volume than most other zone cabling solutions and up to 37% less than traditional twisted pair systems, thereby reducing containment costs and improving airflow in and around the servers and switches. This has the ability to positively impact both initial capital expenditures as well as ongoing operating costs.
  • Density – the MRJ21 XG solution offers 48 RJ45 ports in a fixed, single rack unit configuration, allowing server or switch-specific designs with maximum rack efficiency and minimal wasted space.
  • Throughput – the MRJ21 XG cabling system can be deployed in traditional cross-connect architectures, office LAN environments and the latest server-to-core switch configurations and supports all data rates up to and including 10 Gb/s (Gigabits per second).

The MRJ21 XG copper cabling system offers a number of unique benefits that only TE’s MRJ21 product line can provide. The unique plug design supports four separate 10 GbE transmission channels over a single trunk cable, giving guaranteed throughput performance and fast installation. For higher density copper cross-connect applications, a fixed 48-port 1RU panel is available. Additional benefits include:

  • Supports multiple 10-Gigabit architectures, including top-of-rack (ToR), end-of-row (EoR) and middle-of-row (MoR)
  • Plug-n-play design delivers greater ease of deployment and faster installation of additional capacity/service
  • Supports green IT initiatives by improving airflow and energy efficiency with lower cable volumes
  • Shielded system ensures the highest levels of signal immunity to cross-talk

“Our customers have been asking for this. It’s like having a plug-n-play MRJ21 copper cable system but now for 10 Gb/s vs. 1 Gb/s,” added Patel. “We believe this is a game-changer in the data center industry. Our MRJ21 XG solution is pre-terminated for faster installation, has a sleek and compact design for more efficient use of space, and a high density, multi-channel 10-gigabit connector interface that readies our customers for higher density line cards in the future.” Additional information about the new MRJ21 XG copper cabling system can be found at: www.te.com/MRJ21

About TE Connectivity

TE Connectivity (NYSE: TEL) is a global, $14 billion company that designs and manufactures approximately 500,000 products that connect and protect the flow of power and data inside the products that touch every aspect of our lives. Our nearly 100,000 employees partner with customers in virtually every industry—from consumer electronics, energy and healthcare, to automotive, aerospace and communication networks—enabling smarter, faster, better technologies to connect products to possibilities. For more information, visit: www.te.com.

TE’s Enterprise Networks infrastructure solutions connect people and technology across office networks and data centers. Many of the world’s most complex data networks run applications at speeds of up to 100 Gb/s over products from TE’s AMP NETCONNECT and TrueNet portfolios. For more information, visit: www.TE.com/enterprise.

TE Connectivity, TE connectivity (logo), and MRJ21 are trademarks.

All other logos, products and/ or company names referred to herein might be trademarks of their respective owners.

© 2012 Tyco Electronics Corporation, a TE Connectivity Ltd. company. All rights reserved.

 

Source: TE Connectivity Ltd.

TE Connectivity
Karen Galiger, 336-665-5934
Sr. Communications Manager
Karen.Galiger@te.com
Dave Viertel, 952-917-0454
Product Marketing Manager
Dave.Viertel@te.com