Investor Relations

Email Alerts

Email Address *
Mailing Lists *









Contact IR

Institutional Investors:
Direct Line: 610-893-9435
Click Here to Email

Address:
TE Connectivity
1050 Westlakes Drive
Berwyn, PA 19312

TE Connectivity Main Switchboard:
US 610-893-9800

Connect With Us

Stock Quote

NYSE: TEL $93.62 -0.15 (-0.16%) Volume: 1,226,393 20 minute delay August 21, 2018

TE Connectivity (TE) to Showcase Innovative Medical Solutions at MD&M West 2018

February 05, 2018

TE will highlight its recently expanded portfolio for minimally invasive, surgical, imaging and sensing solutions.

BERWYN, Pa., Feb. 5, 2018 /PRNewswire/ -- TE Connectivity (NYSE: TEL), a world leader in connectivity and sensors, today announced that it will display its portfolio of innovative, efficient and high-performing connectivity and sensor solutions at MD&M West 2018, Booth #3149, Hall D, in Anaheim, California February 6-8, 2018.

TE will showcase its latest medical technology offerings including patient monitoring temperature sensors, photo optic sensors, AD-101 ultrasonic sensors and board level pressure sensors, among minimally invasive, surgical, imaging and other sensor solutions. TE's booth will feature a cath lab simulation experience, allowing visitors to perform a simulated, life-changing clinical procedure.  

TE Connectivity designs and manufactures sensors to specifications needed for the rigors of medical applications, with ISO 13485 certification and FDA registration for various products. Product highlights of the MD&M West 2018 TE display:

  • AD-101 ultrasonic sensors - developed for non-invasive continuous monitoring of fluid for air bubble detection. Using ultrasonic technology, this sensor is capable of positively identifying the presence of a break in flow of any type of liquid.
  • Photo Optic sensors - a key component for non-invasively measuring blood and oxygenation (SpO2) level and suitable for a variety of applications from patient monitoring, to wearables and home healthcare applications.
  • Patient Monitoring 400 series - provide ±0.1°C accuracy per EN-12470 requirements and are compatible NTC patient temperature monitoring sensors.
  • Board level 1620 series - disposable medical pressure sensor measures pressure from -50 to 300mmHG for applications requiring AAMI compliance.

"MD&M West provides us the opportunity to meet with engineers to discuss how TE's extensive sensor and connectivity portfolio can help them optimize the next generation of medical devices," said Mr. Sean Gough, sr. director of sensor product management, TE Connectivity. "TE is proud to be part of the medical device revolution by helping to advance applications ranging from home healthcare to wearable health and mobile medical devices."

TE Connectivity's thousands of engineers provide support of application-specific, standard and custom requirements, from product concept through manufacturing. TE subject matter experts will be on site at MD&M West 2018 to share their insights and discuss engineers' design and manufacturing needs.

ABOUT TE CONNECTIVITY

TE Connectivity Ltd., is a $13 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 78,000 employees, including more than 7,000 engineers, working alongside customers in nearly 150 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedInFacebookWeChat and Twitter.

TE Connectivity, TE and the TE connectivity (logo) are trademarks.
Other company and/or product names might be trademarks of their respective owners.

Contact:

Media Relations:
Keith Myers
TE Connectivity
+1 910 818 0046
Keith.myers@te.com

Cision View original content with multimedia:http://www.prnewswire.com/news-releases/te-connectivity-te-to-showcase-innovative-medical-solutions-at-mdm-west-2018-300593162.html

SOURCE TE Connectivity